RoutingPartLibraryNodeType Enumeration¶
NXOpen.Preferences.RoutingPartLibrary.NodeType is an alias for NXOpen.Preferences.RoutingPartLibraryNodeType
-
class
NXOpen.Preferences.
RoutingPartLibraryNodeType
¶ Bases:
object
Type of nodes in the part library.
Enum Members
Enum Member Enum Member Description Normal Normal node, may contain part table children. Doesn’t have any part table information. Table Part table node. Contains columns/rows that specify parts. Part Part node, contains information necessary for loading/using a routing part. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-