RoutingPartDetailLevel Enumeration¶
NXOpen.Preferences.RoutingPart.DetailLevel is an alias for NXOpen.Preferences.RoutingPartDetailLevel
-
class
NXOpen.Preferences.
RoutingPartDetailLevel
¶ Bases:
object
The detail levels available for the Routing bill of material.
Enum Members
Enum Member Enum Member Description Summary Itemized -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-