RoutingLogicalFlowArrowEnumType Enumeration¶
NXOpen.Preferences.RoutingLogical.FlowArrowEnumType is an alias for NXOpen.Preferences.RoutingLogicalFlowArrowEnumType
-
class
NXOpen.Preferences.
RoutingLogicalFlowArrowEnumType
¶ Bases:
object
How to create terminal segments (if creating terminal segments).
Enum Members
Enum Member Enum Member Description Open Open arrow head on flow arrow. Closed Closed arrow head on flow arrow. Filled Filled arrow head on flow arrow. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-