RoutingApplicationViewAppType Enumeration¶
NXOpen.Preferences.RoutingApplicationView.AppType is an alias for NXOpen.Preferences.RoutingApplicationViewAppType
-
class
NXOpen.Preferences.
RoutingApplicationViewAppType
¶ Bases:
object
Routing application types
Enum Members
Enum Member Enum Member Description NotSet Not currently in any of the routing applications. Mechanical In routing mechanical application. Electrical In routing electrical application. Logical In routing logical application. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-