PostProcessing Class¶
-
class
NXOpen.Preferences.
PostProcessing
¶ Bases:
object
CAE Post Processing preferences
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
NoModelDisplayOnPostviewCreation | Returns or sets the flag which indicates that no finite element model data will displayed when postviews are created |
Methods¶
Property Detail¶
NoModelDisplayOnPostviewCreation¶
-
PostProcessing.
NoModelDisplayOnPostviewCreation
¶ Returns or sets the flag which indicates that no finite element model data will displayed when postviews are created
-------------------------------------
Getter Method
Signature
NoModelDisplayOnPostviewCreation
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NoModelDisplayOnPostviewCreation
Parameters: emptyview (bool) – New in version NX8.0.1.
License requirements: None.