PartVisualizationShadeHiddenShadedFaceEdges Enumeration¶
NXOpen.Preferences.PartVisualizationShade.HiddenShadedFaceEdges is an alias for NXOpen.Preferences.PartVisualizationShadeHiddenShadedFaceEdges
-
class
NXOpen.Preferences.
PartVisualizationShadeHiddenShadedFaceEdges
¶ Bases:
object
Describes whether the shaded face edges are invisible or dashed visible or with a color to depict the hidden geometry
Enum Members
Enum Member Enum Member Description Invisible If selected, shaded face edges that are hidden are not displayed Dashed If selected, hidden shaded face edges are displayed in the body color with a dashed line font. HiddenColor If any color is selected, hidden shaded face edges are displayed in that color. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-