PartVisualizationShadeAdvViewToleranceType Enumeration¶
NXOpen.Preferences.PartVisualizationShade.AdvViewToleranceType is an alias for NXOpen.Preferences.PartVisualizationShadeAdvViewToleranceType
-
class
NXOpen.Preferences.
PartVisualizationShadeAdvViewToleranceType
¶ Bases:
object
Describes the available tolerance types for Advanced View. Each of these options maps tolerance values to for specific operations : Curve Edge Chord Distance, Surface Chord Distance, Angular Tolerance, Facet Width Tolerance
Enum Members
Enum Member Enum Member Description Coarse Coarse Standard Standard Fine Fine Extrafine Extrafine Superfine Superfine Ultrafine Ultrafine Customize Customize. User can specify the Edge Tolerance, Face Tolerance and Angle Tolerance, Width Tolerance specifically. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-