PartVisualizationPerformance Class¶
-
class
NXOpen.Preferences.
PartVisualizationPerformance
¶ Bases:
object
Represents the set of visualization performance preferences applicable to entire part.
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
SaveAdvancedDisplayFacets | Returns or sets the save advanced facets. |
Methods¶
Property Detail¶
SaveAdvancedDisplayFacets¶
-
PartVisualizationPerformance.
SaveAdvancedDisplayFacets
¶ Returns or sets the save advanced facets.
Enable saving of advanced display facets in the part file.
-------------------------------------
Getter Method
Signature
SaveAdvancedDisplayFacets
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveAdvancedDisplayFacets
Parameters: saveAdvancedDisplayFacets (bool) – New in version NX10.0.0.
License requirements: None.