PartVisualizationNamesBordersNameDisplay Enumeration¶
NXOpen.Preferences.PartVisualizationNamesBorders.NameDisplay is an alias for NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay
-
class
NXOpen.Preferences.
PartVisualizationNamesBordersNameDisplay
¶ Bases:
object
Describes the available options for object name display selection
Enum Members
Enum Member Enum Member Description Off Display is Off ViewOfDefinition View of Definition places each name in the work view current at the time of name creation WorkView Work View places all names in the current work view, even if the existing names had been defined in different views AllViews All Views places all names in the all views except the drawing member views -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-