PartVisualizationEmphasisWireframeBlendOptions_Struct Struct¶
NXOpen.Preferences.PartVisualizationEmphasis.WireframeBlendOptions is an alias for NXOpen.Preferences.PartVisualizationEmphasisWireframeBlendOptions_Struct
-
class
NXOpen.Preferences.
PartVisualizationEmphasisWireframeBlendOptions_Struct
¶ Bases:
object
Specifies options that control the color-blending effect used to de-emphasize wireframe geometry.
. Constructor: NXOpen.Preferences.PartVisualizationEmphasis.WireframeBlendOptions()
Fields¶
Field | Description |
---|---|
BlendColor | the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry. |
BlendPercentage | the percentage of the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry It is a value between 10 and 100. |