PartVisualizationEmphasisEdgesType Enumeration¶
NXOpen.Preferences.PartVisualizationEmphasis.EdgesType is an alias for NXOpen.Preferences.PartVisualizationEmphasisEdgesType
-
class
NXOpen.Preferences.
PartVisualizationEmphasisEdgesType
¶ Bases:
object
Determines whether or not edges are displayed for de-emphasized shaded geometry.
Enum Members
Enum Member Enum Member Description Off Displays no edges for de-emphasized shaded geometry. Normal Displays edges for de-emphasized shaded geometry if edges are normally displayed for shaded geometry. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-