PartSheetmetalFlatPatternObjectType Enumeration¶
NXOpen.Preferences.PartSheetmetal.FlatPatternObjectType is an alias for NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
-
class
NXOpen.Preferences.
PartSheetmetalFlatPatternObjectType
¶ Bases:
object
The members of the following enumerated type are used to identify object types to the FlatPattern API. These are not the usual NX object types; they are ordinary NX objects that are known to the flat pattern feature for the type of outline they provide to a bend region, joggle region, or lightening hole.
Enum Members
Enum Member Enum Member Description BendCenterLine Deprecated BendUpCenterLine BendDownCenterLine BendTangentLine OuterMoldLine InnerMoldLine ExteriorCurves InteriorCurves Deprecated InteriorCutoutCurves InteriorFeatureCurves StrikePoint LighteningHoleCenter JoggleLine AddedTopGeometry AddedBottomGeometry ToolMarker -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-