PartObjectObjectType Enumeration¶
NXOpen.Preferences.PartObject.ObjectType is an alias for NXOpen.Preferences.PartObjectObjectType
-
class
NXOpen.Preferences.
PartObjectObjectType
¶ Bases:
object
Describes all available Types for object selection
Enum Members
Enum Member Enum Member Description General Default Type Value Line Line Arc Arc Conic Conic Spline Spline Solidbody Solid Body Sheetbody Sheet Body Datum Datum Point Point CoordinateSystem Coordinate System AllButDefault All But Default DatumCsys Datum CSYS Feature Traceline Traceline InfiniteLine Infinite Line PointCloud Point Cloud -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-