PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions Enumeration¶
NXOpen.Preferences.PartFlexiblePrintedCircuitDesign.FlexibleCableContactFaceOptions is an alias for NXOpen.Preferences.PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions
-
class
NXOpen.Preferences.
PartFlexiblePrintedCircuitDesignFlexibleCableContactFaceOptions
¶ Bases:
object
This enum represents the face that is the contact face of the Flexible Cable.
Enum Members
Enum Member Enum Member Description TopFace Top face. BottomFace Bottom face. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-