GdtOption Enumeration¶
-
class
NXOpen.Preferences.
GdtOption
¶ Bases:
object
Represents the Inherit GD and T options Enum Members
Enum Member Enum Member Description NotSet Does not inherit any GD and T display instances. InDrawingPlane inherit display instances of geometric tolerance features that are parallel to the drawing plane onto the drawing view. FromModelView inherit display instances of geometric tolerance features that exist in a particular modeling view (e.g. Top, Front, etc.). -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-