FlatPatternViewPreferences Class

class NXOpen.Preferences.FlatPatternViewPreferences

Bases: object

Provides access to object and callout properties for sheet-metal data in flat pattern views on drawings.

To obtain an instance of this class, refer to NXOpen.Preferences.ViewPreferences

New in version NX5.0.0.

Methods

Method Description
Commit Commits and applies all the settings done with set_callout_type_display and set_object_type_display.
GetPropertiesObject Returns the properties object for the part’s flat pattern view preferences.

Method Detail

Commit

FlatPatternViewPreferences.Commit

Commits and applies all the settings done with set_callout_type_display and set_object_type_display.

It must be called after a sequence of calls to those methods to cause the view to update.

Signature Commit()

New in version NX5.0.0.

License requirements: nx_sheet_metal (“NX Sheet Metal”)

GetPropertiesObject

FlatPatternViewPreferences.GetPropertiesObject

Returns the properties object for the part’s flat pattern view preferences.

Signature GetPropertiesObject()

Returns:Reference to the object on which to get and set the

preferences for flat pattern drawing member views. :rtype: NXOpen.SheetMetal.FlatPatternSettings

New in version NX5.0.0.

License requirements: nx_sheet_metal (“NX Sheet Metal”)