DetailViewPreferences Class¶
-
class
NXOpen.Preferences.
DetailViewPreferences
¶ Bases:
object
Represents set of Detail View Preferences applicable to drafting views.
To obtain an instance of this class use
Preferences.ViewPreferences.Detail()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CreateIndependent | Returns or sets the toogle create independent |
ViewBoundaryColor | Returns or sets the view boundary color option |
ViewBoundaryFont | Returns or sets the view boundary font option |
ViewBoundaryWidth | Returns or sets the view boundary width option |
Methods¶
Method | Description |
---|---|
SetCircularBoundary | Sets the circular boundary option. |
Property Detail¶
CreateIndependent¶
-
DetailViewPreferences.
CreateIndependent
¶ Returns or sets the toogle create independent
-------------------------------------
Getter Method
Signature
CreateIndependent
Returns: Return type: int New in version NX7.5.3.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
CreateIndependent
Parameters: createIndependentToogle (int) – New in version NX7.5.3.
License requirements: drafting (“DRAFTING”)
ViewBoundaryColor¶
-
DetailViewPreferences.
ViewBoundaryColor
¶ Returns or sets the view boundary color option
-------------------------------------
Getter Method
Signature
ViewBoundaryColor
Returns: Return type: Id New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
ViewBoundaryColor
Parameters: color (Id) – New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
ViewBoundaryFont¶
-
DetailViewPreferences.
ViewBoundaryFont
¶ Returns or sets the view boundary font option
-------------------------------------
Getter Method
Signature
ViewBoundaryFont
Returns: Return type: NXOpen.Preferences.Font
New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
ViewBoundaryFont
Parameters: font ( NXOpen.Preferences.Font
) –New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
ViewBoundaryWidth¶
-
DetailViewPreferences.
ViewBoundaryWidth
¶ Returns or sets the view boundary width option
-------------------------------------
Getter Method
Signature
ViewBoundaryWidth
Returns: Return type: NXOpen.Preferences.Width
New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
-------------------------------------
Setter Method
Signature
ViewBoundaryWidth
Parameters: width ( NXOpen.Preferences.Width
) –New in version NX6.0.2.
License requirements: drafting (“DRAFTING”)
Method Detail¶
SetCircularBoundary¶
-
DetailViewPreferences.
SetCircularBoundary
¶ Sets the circular boundary option.
If True, circular boundary is displayed for detail view, else rectangular boundary is displayed.
Signature
SetCircularBoundary(circularBoundaryOption)
Parameters: circularBoundaryOption (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)