NXOpen.Positioning Package¶
Classes¶
ComponentConstraint Class | Constraint for use in positioning assembly objects in NX. |
ComponentConstraintGroup Class | Constraint group which represents a group of component constraints in NX. |
ComponentConstraintGroupBuilder Class | Represents a NXOpen.Positioning.ComponentConstraintGroupBuilder builder |
ComponentNetwork Class | Network for use in positioning components in NX. |
ComponentPositioner Class | An instance of this class can be used to create :py:class:`NXOpen.Positioning.Constraint`s and associated objects. |
Constraint Class | Constraints for use in positioning objects in NX. |
ConstraintCollection Class | a collection of constraints |
ConstraintReference Class | ConstraintReference for use in positioning objects in NX. |
DisplayedConstraint Class | The displayed representation of a constraint, used for graphical display and to represent it in the Assembly Navigator. |
DisplayedConstraintCollection Class | a collection of displayed constraints |
MatingConverter Class | An instance of this class can be used to convert Mating Conditions to Assembly Constraints in its owning assembly or in child parts of its owning assembly. |
Network Class | Network for use in positioning objects in NX. |
Positioner Class | An instance of this class can be used to create :py:class:`NXOpen.Positioning.Constraint`s and associated objects. |
Enumerations¶
ComponentConstraintDirectionToFixed Enumeration | Specifies how a constraint affects the positioning of a component. |
ComponentConstraintGroupConstraintsCollectionType Enumeration | the enum to define constraint collection type |
ComponentNetworkArrangementsMode Enumeration | Specifies how changes in the network are applied to arrangements. |
ConstraintAlignment Enumeration | Specifies alignment of directed geometries used in a constraint. |
ConstraintSolverStatus Enumeration | Specifies the status of a constraint. |
ConstraintSplineType Enumeration | Specifies how the spline points define the shape of the spline. |
ConstraintType Enumeration | Specifies the type of a constraint. |
ConstraintReferenceConstraintOrder Enumeration | Specifies the order of the constraint reference used in a NXOpen.Positioning.Constraint . |
ConstraintReferenceGeometryType Enumeration | Specifies the type of the geometry used in a NXOpen.Positioning.ConstraintReference . |
ConstraintReferenceHalfSpace Enumeration | Specifies the half space value of one geometry used in a distance constraint. |
MatingConverterPartContext Enumeration | Defines in which parts mating conditions will be converted. |
NetworkObjectStatus Enumeration | Specifies the solver status of a movable object. |