MatingConverterPartContext Enumeration¶
NXOpen.Positioning.MatingConverter.PartContext is an alias for NXOpen.Positioning.MatingConverterPartContext
-
class
NXOpen.Positioning.
MatingConverterPartContext
¶ Bases:
object
Defines in which parts mating conditions will be converted.
Enum Members
Enum Member Enum Member Description InOwningPart Convert mating conditions in the owning part InLoadedChildren Convert mating conditions in the owning part and all loaded children. Partially-loaded children will be fully-loaded. InAllChildren Convert mating conditions in the owning part and all children. Partially-loaded and unloaded children will be fully-loaded. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-