ConstraintSolverStatus Enumeration¶
NXOpen.Positioning.Constraint.SolverStatus is an alias for NXOpen.Positioning.ConstraintSolverStatus
-
class
NXOpen.Positioning.
ConstraintSolverStatus
¶ Bases:
object
Specifies the status of a constraint.
Enum Members
Enum Member Enum Member Description NewlyCreated Not evaluated or suppressed since creation Suppressed Constraint is suppressed OutOfDate Needs evaluation OverConstrained Conflicts with other constraints NotConsistentDims Cannot solve with current dimension values. Model fully defined NotConsistentOther Cannot find a solution. Model underdefined NotConsistentUnknown Cannot find a solution BetweenFixed Attempt to put constraint between two fixed objects NotSolved Not evaluated because other parts of the model are over defined or inconsistent Solved The constraint is solved and satisfied CannotSolve The constraint has invalid geometry and could not be passed to the solver Delayed The constraint is delayed and will not solve IgnoredInArrangement The current arrangement ignores all constraints and they will not solve InternallyInconsistent The constraint references invalid geometry for this constraint type UnloadedGeometry The constraint could not solve as some geometry is unloaded PendingConvertedMc The constraint has been converted from a mating condition and has not solved since conversion ConflictingWithWave The constraint has been suppressed because it’s conflicting with WAVE InconsistentLimits The constraint has limits that are inconsistent and it could not be passed to the solver BeyondLimits The value of the expression of the constraint is beyond its limits and it could not be passed to the solver -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-