ConstraintReferenceConstraintOrder Enumeration¶
NXOpen.Positioning.ConstraintReference.ConstraintOrder is an alias for NXOpen.Positioning.ConstraintReferenceConstraintOrder
-
class
NXOpen.Positioning.
ConstraintReferenceConstraintOrder
¶ Bases:
object
Specifies the order of the constraint reference used in a
NXOpen.Positioning.Constraint
. Typically the order is set during creation, where the first constraint reference added is “outside” and the second “outside”. For Bond constraints, the order is set to be “unknown” at creation.Enum Members
Enum Member Enum Member Description Unknown No order specified Inside Inside Outside Outside -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-