ComponentNetworkArrangementsMode Enumeration¶
NXOpen.Positioning.ComponentNetwork.ArrangementsMode is an alias for NXOpen.Positioning.ComponentNetworkArrangementsMode
-
class
NXOpen.Positioning.
ComponentNetworkArrangementsMode
¶ Bases:
object
Specifies how changes in the network are applied to arrangements. This setting will be ignored when positioning geometry in a piece part.
Enum Members
Enum Member Enum Member Description Existing Apply transforms in arrangements according to existing component properties. Constraints are created non-arrangement specific. InUsed Apply transforms in the used arrangement only. Constraints are created arrangement specific in the used arrangement and suppressed in all other arrangements -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-