PointCollectionPointOnCurveLocationOption Enumeration¶
NXOpen.PointCollection.PointOnCurveLocationOption is an alias for NXOpen.PointCollectionPointOnCurveLocationOption
-
class
NXOpen.
PointCollectionPointOnCurveLocationOption
¶ Bases:
object
Describes whether the input Scalar to the
NXOpen.PointCollection.CreatePoint()
method is a relative percentage parameter or an absolute arc length or a relative percentage arc length.Enum Members
Enum Member Enum Member Description Parameter Scalar is curve parameter. PercentParameter Scalar is a relative percentage parameter. ArcLength Scalar is an absolute arc length. PercentArcLength Scalar is a relative percentage arc length. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-