PointCollectionAlongCurveOption Enumeration¶
NXOpen.PointCollection.AlongCurveOption is an alias for NXOpen.PointCollectionAlongCurveOption
-
class
NXOpen.
PointCollectionAlongCurveOption
¶ Bases:
object
Describes whether the input Scalar to the
NXOpen.PointCollection.CreatePoint()
method is either an absolute distance or a relative percentage.Enum Members
Enum Member Enum Member Description Distance Scalar is an absolute distance. Percent Scalar is a relative percentage. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-