PlaneTypesMethodType Enumeration¶
NXOpen.PlaneTypes.MethodType is an alias for NXOpen.PlaneTypesMethodType
-
class
NXOpen.
PlaneTypesMethodType
¶ Bases:
object
Specifies different method types of selected geometries
Enum Members
Enum Member Enum Member Description Undefined Not defined Inferred Inferred method Coincident Plane of object method CoincidentFaceAxis Though face axis method CoincidentPerpLinear Through linear perpendicluar to linear method Parallel Parallel method ParallelPoint Parallel to plane through point method Perpendicular Perpendicular to plane method PerpendicularPoint Perpendicular to plane though point method PerpendicularLinear Perpendicular to plane through linear method Center Center method Tangent Tangent method TangentFace Tangent to face method TangentPoint Tangent to face through point method TangentLinear Tangent to face through linear method TangentParPlane Tangent to face parallel to plane method TangentPerpPlane Tangent to face perpendicular to plane method TangentTwoFaces Tangent to two faces method TangentAnglePlane Tangent to a cyl face at an angle to a planar face Distance Distance method Angle Angle method Frenet Frenet method PointDir Point and direction method Point Point method TwoPoints Two Points method ThreePoints Three points method Line Line method TwoLines Two line method CurvePoint On curve through point method FixedX Fixed plane perpendicular to X thru WCS FixedY Fixed plane perpendicular to Y thru WCS FixedZ Fixed plane perpendicular to Z thru WCS FixedXyCsys Fixed plane perpendicular to Z thru X-Y plane of CSYS Coefficients Fixed plane defined by coefficients InferredTop Inferred Top method TangentInfer Inferred Tangent method PointInfer Inferred Point method FaceAxisPoint Through Face Axis at Point Fixed Fixed Method (super type including any non-associative, xy, yz, xz, and coefficient FixedView View Plane method Constructed Constructed types: super type for At Angle Parallel/Perpendicular or Tangent Angle to Plane Parallel/Perpendicular -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-