PlaneTypesFrenetSubtype Enumeration¶
NXOpen.PlaneTypes.FrenetSubtype is an alias for NXOpen.PlaneTypesFrenetSubtype
-
class
NXOpen.
PlaneTypesFrenetSubtype
¶ Bases:
object
Specify the subtypes for on_curve type of plane, where alternate solution is not enough to handle the situation after enhancement to this specific plane type. Considering legacy data, these subtypes must match those already defined in the file “datum.h”
Enum Members
Enum Member Enum Member Description NotSpecified Subtype is not specified Tangent Tangent to path, = FRENET_TANGENT Normal Normal to path, = FRENET_NORMAL Binormal Binormal to path, = FRENET_BINORMAL Project Reference to an object, = FRENET_PROJECT ThruPoint Thru point type and normal to path NormalToVector Normal to a vector ParallelToVector Parallel to a vector ThruAxis Thru axis type ThruPointNormalToVector Thru point and normal to a vector ThruPointParallelToVector Thru point and parallel to a vector ThruPointThruAxis Thru point and thru axis type ThruPointNormal Thru point and tangent_to_path ThruPointBinormal Thru point and binormal to path ThruPointProject Thru point and relative to object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-