PhysicalMaterialType Enumeration¶
NXOpen.PhysicalMaterial.Type is an alias for NXOpen.PhysicalMaterialType
-
class
NXOpen.
PhysicalMaterialType
¶ Bases:
object
The different types of materials. The material list generated will be filtered based on the material type chosen
Enum Members
Enum Member Enum Member Description Unknown unknown == error Isotropic Isotropic Orthotropic Orthotropic Anisotropic Anisotropic Fluid Fluid GeneralHyperelastic Hyperelastic - General Mooneyrivlin Mooney Rivlin Mooneyrivlintestdata Mooney Rivlin - test data option Polynomial Polynomial Reducedpolynomial Reduced Polynomial Ogden Ogden Ogdentestdata Ogden - test data option Foam Foam Foamtestdata Foam - test data option Blatz Blatz-Ko Arrudaboyce Arruda-Boyce Arrudaboycetestdata Arruda-Boyce - test data option Neohooke Neo Hooke Neohooketestdata Neo Hooke - test data option Marlow Marlow Vanderwaals Van Der Waals Yeoh Yeoh Yeohtestdata Yeoh - test data option Gent Gent Gasket Gasket Gasketbehavior Gasket Behavior Shapememoryalloy Shape Memory Alloy Sussmanbathe Sussman-Bathe hyperelastic material Gasketdisplacement Gasket with length-based loading Damageinterface Damage interface material Multiplefluid Multiple fluid material Hartsmith Hart-Smith material Alexander Alexander material Curing Curing material Porous Porous material -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-