PhysicalMaterialCategory Enumeration¶
NXOpen.PhysicalMaterial.Category is an alias for NXOpen.PhysicalMaterialCategory
-
class
NXOpen.
PhysicalMaterialCategory
¶ Bases:
object
The different categories of materials. The material list generated will be filtered based on the category
Enum Members
Enum Member Enum Member Description Metals Metals Plastics Plastics Polymers Polymers Ceramics Ceramics Other Other (Not metal, plastic, etc.) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-