PerformanceManagerOutputDevice Enumeration¶
-
class
NXOpen.
PerformanceManagerOutputDevice
¶ Bases:
object
Represents the options to print all the performance statistics information into output device Enum Members
Enum Member Enum Member Description Syslog Print all data to sylog ListingWindow Print all data to listing window Xml Print all data to xml in autotest mode only NotSet No output -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-