PartUnits Enumeration

NXOpen.Part.Units is an alias for NXOpen.PartUnits

class NXOpen.PartUnits

Bases: object

The units of the part file.

Enum Members

Enum Member Enum Member Description
Inches
Millimeters
Mix
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.