PartRelations Enumeration¶
NXOpen.Part.Relations is an alias for NXOpen.PartRelations
-
class
NXOpen.
PartRelations
¶ Bases:
object
The relations of the part file.
New in version NX8.0.0.
Enum Members
Enum Member Enum Member Description Standalone no master model support ReferenceExisting Master model support Mix support any one of relation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-