PartPartFamilyAttrType Enumeration¶
NXOpen.Part.PartFamilyAttrType is an alias for NXOpen.PartPartFamilyAttrType
-
class
NXOpen.
PartPartFamilyAttrType
¶ Bases:
object
The part family attribute types.
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.FamilyAttributeAttrType
insteadEnum Members
Enum Member Enum Member Description TextType text attribute NumericType numeric attribute IntegerType integer attribute DoubleType double attribute StringType string attribute PartType part attribute NameType name attribute InstanceType instance attribute ExpressionType expression attribute MirrorType mirror attribute DensityType density attribute FeatureType feature attribute -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-