PartImporterDestinationCoordinateSystemSpecificationType Enumeration¶
NXOpen.PartImporter.DestinationCoordinateSystemSpecificationType is an alias for NXOpen.PartImporterDestinationCoordinateSystemSpecificationType
-
class
NXOpen.
PartImporterDestinationCoordinateSystemSpecificationType
¶ Bases:
object
Specifies the destination coordinate system specification.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Work Use Work Coordinate System. Specified Use specified coordinate system. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-