PartFamilyMemberData Class¶
-
class
NXOpen.
PartFamilyMemberData
¶ Bases:
NXOpen.TransientObject
This class is responsible for storing part family member data Use the method
NXOpen.Part.NewPartFamilyMemberData()
to create new instance of this class.New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.InstanceDefinition
andNXOpen.PartFamily.TemplateManager
instead.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
SetMemberData | Set the part family member data |
Method Detail¶
Dispose¶
-
PartFamilyMemberData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
Deprecated since version NX9.0.0: PartFamilyMemberData object is deprecated, so dispose of this object is not needed
License requirements: None.
SetMemberData¶
-
PartFamilyMemberData.
SetMemberData
¶ Set the part family member data
Signature
SetMemberData(memberData)
Parameters: memberData (list of NXOpen.PartFamilyMemberValues
) – array of attribute values corresponding to each memberNew in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.PartFamily.TemplateManager.AddInstanceDefinition()
andNXOpen.PartFamily.InstanceDefinition.SetValueOfAttribute()
insteadLicense requirements: None.