PartDisplayPartWorkPartOption Enumeration¶
-
class
NXOpen.
PartDisplayPartWorkPartOption
¶ Bases:
object
Controls what the work part will be when setting active display part. See
NXOpen.PartCollection.SetActiveDisplay()
Enum Members
Enum Member Enum Member Description SameAsDisplay New work part will be set to the new display part UseLast If possible use the work part that was used when this part was last the display part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-