PartCollectionWorkComponentOption Enumeration¶
NXOpen.PartCollection.WorkComponentOption is an alias for NXOpen.PartCollectionWorkComponentOption
-
class
NXOpen.
PartCollectionWorkComponentOption
¶ Bases:
object
Controls the behavior when setting the work component. See
SetWorkComponent()
Enum Members
Enum Member Enum Member Description Visible If the given work component is not visible, chose another component that represents the same part. If no suitable visible component can be found, throw an exception. This option ensures that the new work component will always be visible. Given Use the given work component, regardless of visibility. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-