PartCollectionSdpsStatus Enumeration¶
NXOpen.PartCollection.SdpsStatus is an alias for NXOpen.PartCollectionSdpsStatus
-
class
NXOpen.
PartCollectionSdpsStatus
¶ Bases:
object
Indicates the reason why it was not possible to use Design in Context (i.e. to set the work part to a component of the new active displayed part.)
Used as a return code for
NXOpen.PartCollection.SetDisplay()
Enum Members
Enum Member Enum Member Description Ok The work part was set successfully. This code indicates success: all other codes indicate failure OutsideModelling The modelling application is not active DrawingDisplayed A drawing is currently displayed InPartsList The Part List module is active Gdt The Tolerancing module is active UnitsMismatch The work part and displayed part have different units -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-