PartCleanupDeleteGroups Enumeration¶
NXOpen.PartCleanup.DeleteGroups is an alias for NXOpen.PartCleanupDeleteGroups
-
class
NXOpen.
PartCleanupDeleteGroups
¶ Bases:
object
Which empty groups to clean up
Enum Members
Enum Member Enum Member Description NotSet delete none of the empty groups Unnamed delete only the unnamed empty groups All delete all the empty groups -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-