PartCleanupCleanupParts Enumeration¶
NXOpen.PartCleanup.CleanupParts is an alias for NXOpen.PartCleanupCleanupParts
-
class
NXOpen.
PartCleanupCleanupParts
¶ Bases:
object
Which parts to clean up
Enum Members
Enum Member Enum Member Description Work clean up the work part only Components clean up the work part and its components All clean up all loaded parts -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-