BulkEditBuilder Class |
Represents a BulkEditBuilder to edit bulk of objects. |
DesignContextBuilder Class |
Represents a builder class that performs PID Design Context operations. |
Equipment Class |
Represents the equipment class. |
EquipmentBuilder Class |
Builder used to model a piece of Equipment.
|
FileNewApplicationBuilder Class |
Represents a builder class that performs Generic File New operations. |
FlowDirectionArrow Class |
A symbol that indicates the direction the of the flow
|
FlowDirectionArrowBuilder Class |
Represents FlowDirectionArrowBuilder
|
FlowDirectionArrowCollection Class |
Represents a collection of FlowDirectionArrow. |
LibraryAuthoringBuilder Class |
Represents a LibraryAuthoringBuilder.
|
OffSheetConnector Class |
Represents the off sheet connector class. |
OffSheetConnectorBuilder Class |
Builder used to model a piece of Off Sheet Connector.
|
PidManager Class |
A manager to deal with all objects. |
Pipe Class |
Represents the Pipe class. |
PipeBuilder Class |
Represents a PipeBuilder.
|
Port Class |
Represents the port class. |
PortEquipment Class |
Represents the PortEquipment class. |
PortEquipmentBuilder Class |
Builder used to model a piece of PortEquipment.
|
PreferencesAnnotationBuilder Class |
Represents a PreferencesAnnotationBuilder |
PreferencesBuilder Class |
Represents a PreferencesBuilder |
PreferencesConnectionBuilder Class |
Represents a PreferencesConnectionBuilder |
PreferencesGeneralBuilder Class |
Represents a PreferencesGeneralBuilder |
PreferencesOffSheetConnectorBuilder Class |
Represents a PreferencesOffSheetConnectorBuilder |
Sheet Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
SheetTemplateBuilder Class |
Represents a NXOpen.PID.SheetTemplateBuilder builder, and the builder is used to model a sheet template. |