PreferencesConnectionBuilder Class¶
Properties¶
Property | Description |
---|---|
AllowNonOrthogonalConnections | Returns or sets the allow non-orthogonal connections. |
ArrowSize | Returns or sets the arrow size. |
ArrowStyle | Returns or sets the arrow style. |
JumperGap | Returns or sets the jumper gap. |
JumperPriority | Returns or sets the jumper priority type. |
JumperPriorityUseLineType | Returns or sets the jumper priority use line type. |
JumperType | Returns or sets the jumper type. |
MinimumSegmentLength | Returns or sets the minimum segment length. |
SnapAngle | Returns or sets the snap angle |
Tag | Returns the Tag for this object. |
TeeSize | Returns or sets the tee size. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |