PreferencesAnnotationBuilder Class¶
Properties¶
Property | Description |
---|---|
ConnectionLabelHorizontalOffsetPosition | Returns or sets the horizontal position of the connection tag. |
ConnectionLabelOffset | Returns or sets the gap between the connection and the tag. |
ConnectionLabelPositionCenter | Returns or sets the tag is displayed at the center of the connection. |
ConnectionLabelVerticalOffsetPosition | Returns or sets the vertical position of the connection tag. |
TablesCellSettings | Returns the preferences tabular note settings builder |
Tag | Returns the Tag for this object. |
TextStyleConnectionBuilder | Returns the connection text style of the Annotation. |
TextStyleNoteBuilder | Returns the note text style of the Annotation. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |