Commit |
Commits any edits that have been applied to the builder. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
GetBendPoints |
Get bending points for polyline to render the connection. |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnection |
Get the connection object of the connection builder. |
GetEnd |
Gets the end port of this pipe. |
GetEndLocation |
Get the end location of this connection. |
GetEndTee |
Gets the end Tee. |
GetEndTeeLocation |
Get the connection location for tee object at the end of the connection. |
GetNewEndTeeConnection |
Gets new connection after inserting the end Tee. |
GetNewStartTeeConnection |
Gets new connection after inserting the start Tee. |
GetObject |
Returns the object currently being edited by this builder. |
GetStart |
Gets the start port of this connection. |
GetStartLocation |
Get the start location of this connection. |
GetStartTee |
Gets the start Tee. |
GetStartTeeLocation |
Get the connection location for tee object at the start of the connection. |
SetBendPoints |
Set bending points for polyline to render the connection. |
SetEnd |
Sets the end port of this pipe. |
SetEndLocation |
Set the end location of this connection. |
SetEndTeeLocation |
Set the connection location for tee object at the end of the connection. |
SetStart |
Sets the start port of this connection. |
SetStartLocation |
Set the start location of this connection. |
SetStartTeeLocation |
Set the connection location for tee object at the start of the connection. |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |