OffSheetConnectorBuilder Class
Properties
Property |
Description |
ElementId |
Returns or sets the current element ID of this OSC. |
Horizontal |
Returns the option to flip the symbol horizontally. |
OwningSheet |
Returns or sets the owning sheet of this sheet element. |
RotateOption |
Returns or sets the symbol rotation angle. |
Style |
Returns or sets the style of OSC |
Tag |
Returns the Tag for this object. |
TextStyleBuilder |
Returns the text style of the OSC. |
Vertical |
Returns the option to flip the symbol vertically. |
Methods
Method |
Description |
Commit |
Commits any edits that have been applied to the builder. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
FlipHorizontally |
To flip a off sheet connector horizonally |
FlipVertically |
To flip a off sheet connector vertically |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnection |
To get the connection connecting to the OSC sheet element. |
GetLocation |
Gets the symbol location. |
GetNode |
Get the node object of the off sheet connector builder. |
GetObject |
Returns the object currently being edited by this builder. |
LinkOSC |
Links to the destination OSC. |
Rotate |
To rotate a off sheet connector |
SetConnection |
To set the connection connecting to the OSC sheet element. |
SetLocation |
Sets the symbol location. |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail
ElementId
Horizontal
OwningSheet
RotateOption
Style
TextStyleBuilder
Vertical
Method Detail
FlipHorizontally
FlipVertically
GetConnection
GetLocation
GetNode
LinkOSC
Rotate
SetConnection
SetLocation
Validate