FlowDirectionArrowBuilder Class
Properties
Property |
Description |
LocationPercent |
Returns or sets the percent along the segment for this Flow Direction Arrow. |
LocationSegment |
Returns or sets the segment this Flow Direction Arrow is located on. |
Tag |
Returns the Tag for this object. |
Methods
Method |
Description |
Commit |
Commits any edits that have been applied to the builder. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnection |
Gets the connection for this Flow Direction Arrow. |
GetObject |
Returns the object currently being edited by this builder. |
ReverseDirection |
Change the direction of FDA. |
SetConnection |
Sets the connection for this Flow Direction Arrow. |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail
LocationPercent
LocationSegment
Method Detail
GetConnection
ReverseDirection
SetConnection
Validate