FileNewApplicationBuilder Class
Properties
Property |
Description |
DisplayPartOption |
Returns or sets the display part option for the new file being created |
Tag |
Returns the Tag for this object. |
TemplateBaseTcType |
Returns or sets the BaseTCType of the template part from which to create the new file |
TemplateFileName |
Returns or sets the name of the template part from which to create the new file |
TemplatePresentationName |
Returns or sets the presentation name of the underlying template which is used for creating new file |
TemplateTcType |
Returns or sets the TCType of the template part from which to create the new file |
TemplateType |
Returns or sets the template type for the new file being created |
TemplateUnits |
Returns or sets the units for the new file being created |
Property Detail
DisplayPartOption
TemplateBaseTcType
TemplateFileName
TemplatePresentationName
TemplateTcType
TemplateType
TemplateUnits
Method Detail
AutoAssignAttributes
AutoAssignAttributesWithNamingPattern
CreateAttributeTitleToNamingPatternMap
GetCollaborativeDesign
GetTargetPartitions
SetCollaborativeDesign
SetTargetPartitions
Validate