SmartSaveBuilderSaveType Enumeration¶
NXOpen.PDM.SmartSaveBuilder.SaveType is an alias for NXOpen.PDM.SmartSaveBuilderSaveType
-
class
NXOpen.PDM.
SmartSaveBuilderSaveType
¶ Bases:
object
Represents an File Save type
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Save File Save SaveAll File SaveAll SavePreciseAssembly File SavePreciseAssembly SaveWorkPartOnly File SaveWorkPartOnly SaveAndClose File Save And Close SaveDesignElements Save Design Elements -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-