SaveAsReviseCallbackData Class¶
-
class
NXOpen.PDM.
SaveAsReviseCallbackData
¶ Bases:
NXOpen.TaggedObject
JA interface for SaveAsReviseCallbackData object
This cannot be created
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
GetCopiedObjects | Gets the source objects tags along with copied objects tags after saveas or revise operation |
GetSourceObjects | Gets the source objects tags participating in saveas or revise operation |
Method Detail¶
GetCopiedObjects¶
-
SaveAsReviseCallbackData.
GetCopiedObjects
¶ Gets the source objects tags along with copied objects tags after saveas or revise operation
Signature
GetCopiedObjects(sourceObjects)
Parameters: sourceObjects ( NXOpen.TaggedObject
) – tag of source object for which copied objects are requiredReturns: array of copied objects to be saveas or revise Return type: list of NXOpen.TaggedObject
New in version NX11.0.0.
License requirements: None.
GetSourceObjects¶
-
SaveAsReviseCallbackData.
GetSourceObjects
¶ Gets the source objects tags participating in saveas or revise operation
Signature
GetSourceObjects()
Returns: a tuple Return type: A tuple consisting of (nObjects, sourceObjects). nObjects is a int. get number of source objects going for SaveAs or Revise sourceObjects is a list of NXOpen.TaggedObject
. array of source objects to be saveas or reviseNew in version NX11.0.0.
License requirements: None.