PdmFile Class¶
-
class
NXOpen.PDM.
PdmFile
¶ Bases:
NXOpen.TransientObject
Contains methods for accessing PDM file data.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetFileLastModifiedDate | Get the last modified date of a PDM file. |
GetFileName | Get the file name of a PDM file. |
GetFileSize | Get the file size of a PDM file. |
Method Detail¶
Dispose¶
-
PdmFile.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetFileLastModifiedDate¶
-
PdmFile.
GetFileLastModifiedDate
¶ Get the last modified date of a PDM file.
Signature
GetFileLastModifiedDate()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.