PartOperationImportBuilderValidationRuleSetFileBrowseOption Enumeration

NXOpen.PDM.PartOperationImportBuilder.ValidationRuleSetFileBrowseOption is an alias for NXOpen.PDM.PartOperationImportBuilderValidationRuleSetFileBrowseOption

class NXOpen.PDM.PartOperationImportBuilderValidationRuleSetFileBrowseOption

Bases: object

This enum is used to specify the option to browse the validation rule set file from.

Enum Members

Enum Member Enum Member Description
Native
Teamcenter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.